This is my first post and I apologize in advance if this is not the right place to post this topic.
I am looking for PMSM application notes, for 2808, using FOC with QEP.
So far I have found "sprc212" and "sprc129". From the descriptions of the application…
Other Parts Discussed in Thread: CONTROLSUITE Hi,
I have a question about the 'CalibrationAngle' variable tuning method of the PMSM sensored control examples.
What is the difference between the 'F280x PMSM3_4' example's 'CalibrationAngle' variable…
Other Parts Discussed in Thread: CONTROLSUITE Hi,
I look at sprc179 and sprc212 application software for F280x sensored position controll of 3-phase PMSM using QEP.
Did you have source and document about sensored position controll of 3-phase PMSM using…
Hi,
I am trying to build a PMSM servo application based on the DRV8312-C2-KIT with F28035 Piccolo controlCARD. I found an example code for HVMotorCtrl+PfcKit_v2.0 for running HVPM in sensored servo mode. I would like to port it to the DRV8312-C2-KIT.…
I`ve implemented changes to HVPM_sensored project on TMDSHVMTRPFCKIT and HVPMSMMTR, according sprc179/sprc212. I purged speed_fr macro and added loop from Mechtheta to Iqref via P regulator (Kp is big, around 20 as in example) with constant PositionRef…
I`ve implemented changes to HVPM_sensored project (to make PMSM position control) on TMDSHVMTRPFCKIT and HVPMSMMTR , according sprc179 / sprc212 . I purged speed_fr macro and added loop from Mechtheta to Iqref via P regulator (Kp is big, around 20 as in example…
Cho,
For FOC speed control using encoder you should use
C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v124\PM_Sensorless
Note that through level 6 an encoder is used to verify and tune the sliding mode observer sensorless algorithm
We used e…
I am using SPRC212 (PMSM), the original application is for CCS3 and I have imported it to CCS4.
After importing the "includes" were not pointing correctly, this I fixed by including path using the "C/C++build > Tool Setting > Include Options". Also some…