Hi Isha,
Starterware package is an hardware abstraction layer that applies only to C6747, C6748 and OMAPL, AM335x devices. C672x devices supports a hardware abstraction layer that is called chip support library (CSL) which you can download here:
http…
Sajaad Boodoo,
Welcome to the TI E2E forum. I hope you will find many good answers here. In addition you can find some details through the TI.com documents and the TI Wiki Pages. Be sure to search those for helpful information and to browse for the questions…
Hi Michael,
Are you using the CSL provided below in your code? If not you might want to consider using that package which has been tested and verified.
http://focus.ti.com/docs/toolsw/folders/print/sprc223.html
Jeff
Other Parts Discussed in Thread: SPRC223 I am looking for initialization and McASP setup for stereo in and out. More specifically example code for this.
THank you,
Frank
Why this link is failured? http://e2e.ti.com/forums/p/906/2734.aspx#2734 And i find there has any error on dMax serviced to SPI slave too:
1) CSL_dmaxHwSetup() can not well configure SPI dMax and will generate error code "-67" meaning fault etype.…
I have no idea what you have downloaded, but "applypatch.obj" is not the right file. You should have downloaded sprc203 and sprc223.
Which version of CCS and which version of Code Generation build tools are you using?
Other Parts Discussed in Thread: SPRC223 , SPRC121 , SPRC203 Grtns,
Anyone with knowledge re. CCS4p1p1 compatibility with sprc203_v2, sprc223_v04 and sprc121_ v2.0, please advise.
Regards,
Other Parts Discussed in Thread: SPRC223 Basically what I'd like to do is to create an interrupt using the RTI timer. Details follow.
I'd like to, if I can, count how many McASP receive operations have happened and interrupt the CPU when the count…
Joseph Zolyak said: The puzzling aspect is that the DSP code gets stuck at the EXACT SAME point inside the CSL_intcHookIsr routine, looping between addresses 80050F50 and 80050F60, regardless of which set of tools generated the code.
So are you saying…