Part Number: SRC4193 Hi,
Could you please let me know if there are any disadvantages when LGRP is set to "1" (low group delay)? For example, SNR, distortion, sound quality, etc.
Best regards, Kato
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Hi,
Could you please let me know any differences and any time constraints required between the the hard mute by using pin 14 and the soft mute via SPI port? Additionally, is the hard mute function…
Part Number: SRC4193 Hi Team,
Could you help to confirm if SRC4193 support I2C control? We notice I2C is mentioned in 8.2.1 section, but we don't know which pin are assigned to I2C, also don't know the I2C slave address. Please help to confirm, thanks…
Part Number: SRC4193 Hello,
we have xmos based usb audio interface board with flip flop recloking then we send i2s signal to sample rate converter for upscale sample rate.
So the recloking before SRC is useless or it has a positive effect to get more…
Part Number: SRC4192 Other Parts Discussed in Thread: SRC4193 , PCM5242 Hi,
For the SRC4193, the decimation filter can be enabled or disabled by setting the DFLT, but is my understanding correct that the decimation filter for the SRC4192 can only be enabled…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Does SRC419x support I2S 16bit input data format? I saw the same question but the answer repeated its pdf that has not clear description for I2S mode. So I need just the simple answer yes or…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Will the SRC4193 or SRC4192 work with a 16 bit I2S input? The documentation is a little confusing. It talks generally about working with 24 bit I2S and 24 bit left justified input, but doesn…
Part Number: SRC4193 Hello,
When doing volume control with the SRC4193 how many bits does it use internally for volume control 32, 64? This is not mentioned in the datasheet.
Thanks;
Leo
Part Number: SRC4193 Hi,
I am considering using one of the SRC419x devices, it will have variable bit depth and sampling rates in but I want the output locked to 16bit 44.1KHz, is it possible to detect when the input is the same as the locked output…