Hi Richard,
As far as the SRC4194 EVM goes, the EVM was designed long time ago and it has DIT/DIR/PLL to configure the input and the output clock/data for the SRC. Hence we do have different configuration for the clock/data sources for input/output…
Other Parts Discussed in Thread: SRC4194 Hi,
Could you please tell us whether we can obtain each audio output as the synchronous output by setting the registers of SCR4194 if the audio sources of the different sampling rates are input to SRC4194 and…
Other Parts Discussed in Thread: SRC4194 Hi,
I'm using the SRC4194 in software mode, but am unsure whether the unused hardware mode select pins should simply be left floating or tied to GND or VDD?
Many Thanks,
Mark
TSL Products Ltd.
Hello Kuramochi-san,
Yes, the SRC4184 and SRC4194 are functionally equivalent except the specifications are better (144 vs 128dB) for the SRC4194.
When the output ports are configured in Master mode then they will continue to clock out information…
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: PCM3168A , SRC4392 , SRC4382 , DIX4192 , SRC4184 , DIX9211 , SRC4194 Hi Sir,
My customer is looking for an Audio Codec device and request spec as below.
1. 4 serial in 4 serial out, I2S and…
Part Number: SRC4194EVM Other Parts Discussed in Thread: SRC4194 I'm trying to use the SRC4194 eval kit in a mode where the SRC chip is acting as a slave on both the input and the output. I'm only using the port A, and the B port is unused.
I'm trying…
Hi James,
I'm not able to find information on all of the devices above but these seem to largely be part of AKMs multi-channel DSP integrated Codecs. Unfortunately we do not have single chip solutions that can replace these devices, but it may still…