Hi Henry,
From your post they are using the part as Slave mode, which means they send the I2S from an external source and thus whatever they select to send, the Part will receive it. With same token, if the output port is also in slave mode, then they have…
Part Number: SRC4392 Hello,
Is the SRC4392 capable of receiving S/PDIF over TOSLINK with varying frequency, for example 44.1kHz or 48kHz and using an internal clock source from our system to transmit S/PDIF over TOSLINK with a fixed frequency?
I.e. receive…
Hi Jan,
I connect the computer (that has PPC3 installed on it) via usb to the board/EVM (that has the device on it) and write the script using PPC3.
Reg0x01 turns on all blocks, the configuration of each block can be achieved by their own dedicated registers…
Part Number: SRC4392 I have a current product with 4 CS8422 SRC , which is now obsolete. I am looking into replacing the all 4 CS8422 with the SRC 4192.
The current configuration is the product has 4 AES3 inputs and 4 AES outputs (CS8406) with the AES3…
Part Number: SRC4392 We are designing a board using 4 x SRC4392, all as both DIR and DIT. We would like to make sure the DIT outputs of all 4 devices are synchronised (the source data will have the same MCLK, BCLK, LRCLK).
From the datasheet it looks…
Hi Christian,
I will leave the office shortly and will come back on the 17th of July. So if you want wait until i come back
I will work on it as my schedule permits, so it might take a while but I don't promise that I can solve the issue, as I think you…
Part Number: SRC4392
I was wondering how much (in ppm for example) the MCLK frequency is allowed to deviate from the value set in Register 11: PLL1 Configuration Register 3 when used as reference for DIR.
Part Number: SRC4392 Hello,
I may be a little dull, but I can't quite figure out how to configure the SRC4392 in a manner in which I could convert I2S @ 48 kHz to S/PDIF @ 44.1 kHz.
I looked at the PLL1 and PLL2, but things got a bit muddy there…
Part Number: SRC4392 1, register 01 Does only a transmitter not have any problem in PDALL=0, PDPA=1, PDRX=1 at time to use only time PDALL=0, PDPA=1, PDTX=1 receiver to use? Please reply it whether there is a problem (others without mention are 0)
2,…
Part Number: SRC4392 We have successfully used every single feature of this device..... except channel status for the DIT.
We are changing pages. We are reading interrupts. We are receiving the Tx Complete interrupt exactly as expected. We have tried…