Part Number: DK-TM4C123G DK-TM4C123G: No data at SDout SPI interface to ADC TLV5608 & DAC TLV1570
hi , I m currenting using STM32H7 to interface to TI ADC TLV1570 & TLV5608, I manage to get the SPI working on STM32H7 i m able to transmit and receive…
Ashley Brown said: I was able to test with a Hello Example project and that worked, so I am back to where I was in the beginning but slightly more confused.
Hi Ashley,
This confirms that DK board is in good condition. If the on board ICDI is bad, you…
Part Number: DK-TM4C123G Hi I m working on STM32H7 MCU that use TI TLV5608 & TLV1570 ADC DAC for data collection, i would like to request sample code on any MCU eg. MSP430 or TM4C123G interfacing to both ADC/ DAC (TLV5608 & TLV1570 ADC DAC) using SPI…
Part Number: SW-DK-TM4C129X Hi TI-team,
I would like to use the lwIP TCP/IP stack to implement a Modbus TCP/IP protocol on a TM4C129X or MSP432 microcontroller.
I have a DK-TM4C129X development board and went through some examples like the "Ethernet with…
Part Number: DK-TM4C123G Hi team,
Here's an issue from the customer may need your help:
Unlocking PF0 requires the following three lines, but it is not clear how to write to unlock:
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE…
Part Number: SW-DK-TM4C129X Hello!
I have an Graphic LCD display application to be implemented. So I am using DK-TM4C129x for the same. I wanted to display various input and output data coming from my external devices that will be connected to the development…
Part Number: SW-DK-TM4C123G Other Parts Discussed in Thread: EK-TM4C1294XL Hi All,
I am having a hard time getting a simple PWM period measure program to work and need some help.
I am supplying a 320Hz PWM to port PL0 and I want to use a capture event…
Hi,
I tried the sd-card example for dk-tm4c129x and it is working out of the box for me. This means the example and the FAT file system are working. You will need to port the example to TM4C123. There is also the sd-card example for a obsolete TM4C123…
Part Number: DK-TM4C123G hello ,
I was able to run the program which were given in the tivaware examples in DK-TM4C123GH6PGE . But while creating new project for graphics example i am getting
#1965 cannot open source file "drivers/cfal96x64x16.h"…
Zeynep,
If you look into Resource Explorer, you will see a section for the TM4C ARM devices. In this folder you can find the examples for the TM4C123.
You can also get there from dev.ti.com:
https://dev.ti.com/tirex/explore/node?devtools=DK-TM4C123G&node…