Part Number: BQ78PL11XAPI-SW Other Parts Discussed in Thread: BQWIZARD
Hello,
I am currently facing an issue using the bq78pl11x API. Specifically, the bq78pl11x API demo does not recognize or find the USB to GPIO adapter when attempting to discover the…
Part Number: SW-TM4C Other Parts Discussed in Thread: TM4C129ENCZAD , EK-TM4C1294XL
I loaded the USB_dev_bulk folder in SW-TM4C into TM4C129ENCZAD. (Created a project in CCS and through the XDS110 Debugger.)
The USB device was recognized as unknown after…
Part Number: SW-TM4C Other Parts Discussed in Thread: TM4C129ENCZAD , Hello TI Engineers As soon as possible, I would like to use dfuprog.exe to open the USB port of TM4C129ENCZAD.Is it possible?
If possible, please tell me the command input and procedure…
Hello Kanematu-san,
Not 100% accurate.
Hiroyuki Kanematu said: It means that the program can be written to the IC in Virgin state without using <IC name.h>.
Correct.
Hiroyuki Kanematu said: However, <IC name.h> and peripheral.h cannot be used at the…
Part Number: TUSB8020B I have seen multiple entiries asking for the tools to configure the device over USB. Is this not normally a supported mode? Why not publish this and the EEPROM programming tool (if different) on the device web page?
I am needing…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: USB2ANY Hi Experts,
Asking your assistance on this query about TICSPRO-SW. For this tool, can we use a USB to I2C adapter other than a USBTOANY adapter? Customer has Aadvark adapter to use USB to…
Part Number: LMK03318 Other Parts Discussed in Thread: USB2ANY Hi
I would like to know if I can configure my on board PLL via the TICS Pro SW and USB to I2C Elite programmer
( https://i2ctools.com/product/usb-to-i2c-elite/ )
Regards
Omer
Part Number: SW-TM4C
After evaluation of the TivaWare UsbLib and using TI's offered USB example projects, I want to reuse TI's USB Vendor Identification Number (VID) and USB Product Identification Numbers (PID) for my final product. Is this possible…
Part Number: BQ25616 Dear Teams,
My customer is using BQ25616, and here is the schematic diagram:
1. The USB signal of bq25616 is directly connected to the type C interface. The power supply can use 1.2A to charge the battery.
2. After the usb signal…
Part Number: DP83867IRPAP-EVM Other Parts Discussed in Thread: USB-2-MDIO , MSP-EXP430G2ET , UNIFLASH Hello team,
My customer is trying to set PHY configuration via USB-2-MDIO SW Tool.
Could My customer checked the MDC waveform.
However, customer sees the…