Part Number: TAS2552 Other Parts Discussed in Thread: TAS2563 Hello,
I have designed a system that is composed of two devices with audio output (master/slave).
The system is now on production however now it started to appear reports of some units with…
Part Number: TAS2552 Hi Team,
We are seeking your help regarding our customer's inquiry below.
I have a question regarding the tas2552 edge rate (register 0x13). When I set the default value in the tas2552.c driver it does not seem to respect the…
Part Number: TAS2552 Hi,
I got a request from customer and the request is to fix the output power to 1.5W.
The designed input is i2s.
Can it be controled by register setting?
Thanks.
Part Number: TAS2552 Hi TI Team,
I encountered a problem when debugging TAS2552. When the sound is adjusted to the maximum, there will be a stuck phenomenon.
At the same time, it is verified that this situation still exists in the TI TAS2552 EVM.
Part Number: TAS2552 Other Parts Discussed in Thread: TAS2562 , Hi Ti Team,
Can TAS2552 directly use TAS2562 software? Currently there is no sound using TAS2562 software.
Below is the schematic diagram of TAS2552. Please help to check whether there is any…
Part Number: TAS2552 Now I use TAS2552 in imx6Q,
Now there was a very strange phenomenon, after each equipment to the electricity, the playback of audio, there is no sound out, then continued to put after a period of time (hours are not fixed), the horn…
Part Number: TAS2552 Other Parts Discussed in Thread: TAS2555 , , TAS2557 , TAS2559
hi,
please help give PPC3 right of( TAS2552/TAS2555/ TAS2557 / TAS2559 ) to customer account liuxiequan@cvte.com 、 huangxiongfei@cvte.comand my account eric-zhudg@ti.com
Part Number: TAS2552 Hi Experts,
customer complain audio drop of TAS2552 at 3W/4R output, and I found TAS2552 EVM can repeat audio drop issue when playing music at at below condition:
VBAT=4V , IOVDD=DVDD=1.8V, speaker=4ohm. signal input from AP I2S,…
Part Number: TAS2552 Other Parts Discussed in Thread: TAS2505-Q1 Dear all,
In order to design a short to Vbat protection circuit for class D amplifier output, I would need to know after how much time the devices would be damaged if a short to Vbat occurs…