Part Number: TAS2562
Dear Support,
For TAS2562 device, can I know if my bit clock is fixed at 3MHz and frame SYNC is 44.1Khz. Any requirement and rule to follow for bitclock in respect to FRAME SYNC?
Must it be sync?
Best regards,
kpk
Hi Chris,
I was checking this on the EVM and the limiter was working as expected. as VBAT was decreasing below the inflection point the output voltage was decreasing as well. which is the only function of the limiter to prevent brownout.
if you use a…
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2562 Hi team,
I believe the difference between TAS2562 and TAS2563 is that they have DSP or not, is that correct? Can I assume that all other parts of the device are equivalent?
Sincerely, Ryu
Part Number: TAS2562
Dear Expert,
I would like to know the specifications about TAS2562 Please teach us about TAS2562 of Audio Amplifier.
We designed our equipment using TAS2562 for Audio spearker.
I have a speaker connected to the TAS2562 and am outputting…
Part Number: TAS2562 Hi team,
Customer plan to use TAS2562.
They plan to connect 5V to both VABT and PVDD. This should be OK for their application, right?
They checked the following figure, only get PVDD4.5V waveform.
They would check about the output…
Part Number: TAS2562 Other Parts Discussed in Thread: CC8530 , , , TAS2563 Hello,
One of our new products has a custom PCB using 2 TAS2562s and a CC8530. The chip gets stuck in a startup loop because the i2c bus is not working. I have included a scope capture…
Part Number: TAS2562 Hi TI Team,
I'm using TAS2562 Speaker amplifier and 10mW speaker connected to it.
Issue is at some particular sound the sound get saturated .output from speaker didnt get .
Could you explain what can be the reason for it…
Part Number: TAS2562 Other Parts Discussed in Thread: CC8530 , TAS2557 , TAS2781 , TAS2563 Is it possible to tune a smart amp with the purepath console 3 software through the CC8530 chip? I have just about finished the xml file to integrate the TAS2562 in…