Carlos,
What power level do you need? It looks like you're designing for ~300W Mono.
You are correct that the TAS5261/TAS5624 devices accept only PWM input and not PCM input. That being said, you have a few options.
1. Use one of our PCM Audio…
Other Parts Discussed in Thread: TAS5704 , TAS5601 , TAS5086 Hi,
Currently our customer uses TAS5704 with TAS5601 as D-AMP for subwoofer.
According to the TAS5704 datasheet page 2, connection between TAS5704 and TAS5601 in BTL mode is as follows.
TAS5601…
Other Parts Discussed in Thread: TAS5630B HELLO, I WOULD LIKE TO USE THE AMPLIFIER TAS5630B or the TAS5261 and I would like to know which DC / DC converter advise me to use this integrated in a car with voltage 12/24 V battery. I have identified the LM5122MH…
Kim,
"There is a implementation of volume control than does not reduce the dynamic range: PSVC as used in the TAS5508C with an open loop powerstage like tas5261"
as far as I understand the things, PSVC used in systems based on TAS5508C modulator…
Hi Paul-san,
Thank you for your quick response. The conditions are shown as below.
Pout : 80W ~ 120W(non-clipping output voltage) Rload : 4Ω PVDD_X : 28V ~ 36V Output Configuration : BTL
Could you please tell us "the gain variation vs the power supply…
Other Parts Discussed in Thread: TAS5631 In the Mid/High-Power Amplifier product selection guide, a distinction is made between open-loop and closed-loop power stages. For example, the TAS5631 is "closed-loop", whereas the TAS5261 is "open-loop". I couldn…
There is a DKD 36 pin PSOP3 package in the library Texas.lbr if that's your package It's related to the device TAS5261 You should be able to copy and adapt that part for your use. There are good tutorials on the web to learn how to create library…
Hello Don,
in order to verify the differences I had two experienced listeners in a blind test today. As I'm working under NDA I can't tell the company. They are audiophile loudspeaker producers and the equippment was in their listening room with their…
Other Parts Discussed in Thread: PCM2706 , CC8520 I have built a design based on the CC8520 wireless audio streaming IC, the PCM2706 USB audio interface, and the TAS5261 class D amplifier output stage. The system interfaces a PC's USB port with a TAS5261…
Other Parts Discussed in Thread: TAS5086 HI, I am using DRV8432 as in following ckt. But I always got a 0.5Vpp 384k Hz noise at OUT-A and OUT-B, even I fed the DRV8432 with 50% duty cycle PWM signal form a signal generator(The PWM generator IC used is…