Hello all,
I'm working with the TAS5518-5261K2EVM I've had for quite a few years now, and at some point during one of a couple moves, I've lost the CD-ROM that came with the kit. Does anyone know if a replacement CD-ROM can be ordered from…
Other Parts Discussed in Thread: TAS5518 , CC8531 , TAS5518C I would like to ask regarding this PWM codec.
I need to use 300W amplifier by using TAS5631PHD evaluation module. As I look into Purepath wireless configurator, TAS5518 was available in device…
Hi Marvin,
The TLV320ADC3101 is specified inside https://www.ti.com/tool/PUREPATH-WL-CFG since that's what the CC85XXDK(-Headset) supports in its hardware design, however the datasheet and TRM does clarify that other TI audio devices supporting serial…
Other Parts Discussed in Thread: TAS5518 We have seen the TAS5518 output DC. We have not been able to duplicate this except by using a spdif source that we can set a DC offset into and making all the bi quads pass through.
Is there any setting we can inadvertently…
We have seen the TAS5518 output DC. We have not been able to duplicate this except by using a spdif source that we can set a DC offset into and making all the bi quads pass through.
Is there any setting we can inadvertently set that would allow the TAS5518…
Other Parts Discussed in Thread: TAS5518 , TAS5508C , TAS5518C I have used TAS5518. but 5518 is NRND.
so I try to change TAS5518 to TAS5508C.
what's the differences between TAS5518 and TAS5508C ?
Other Parts Discussed in Thread: TAS5518 , CC8520 I am studying a project that would use 6 to 8 digital mics and a CC85xx. The TAS5518 CODEC looks ideal and the PurePath Configurator supports it. Unfortunately, the TAS5518 is marked as not suitable for…
Other Parts Discussed in Thread: TAS5518 , TAS5508C Hi folks
i was wondering if I can get some info from TI gurus regarding Tas5518.
Gone thru the data sheet in detailed and can't really figure out how the dynamic range is 110dB. Looking at the architecture…
Other Parts Discussed in Thread: TAS5518 , TAS5630B , TAS5630PHD2EVM I would like to drive 32 Vrms into a 10 ohm load with the EVM ~ 108 W. Can I connect the L & R channel together to increase the max power? I would like to drive load with minimum distortion…
Other Parts Discussed in Thread: TAS5518 Hello.
I'm going to build an amplifier based on the TAS5518 processor.
I'm having troubles to find an application schematic that converts the 5518 PWM Headphones output to Analog signal to feed into a TPA6120A…