Part Number: TAS5713 Hi team,
One of our customer's issues, could you please provide some troubleshooting suggestions
I am trying to program the DRC on the TAS5713.
The documentation says the threshold is in 9.23 format and the other coefficients…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5713 , TAS5825M , TAS5822M , TAS5805M
Hello. I'm trying to configure the TAS5731M Amplifier, but I can only initialize it, but nothing sounds. It goes from 0mA to 45mA when I start it, but I don…
Part Number: TAS5713 Hi
My KMM customer use TAS5713 and meet the audio output is not stable. sometime is no output.
so they found the register 0x02(ERROR STATUS REGISTER),value is 0x40 (PLL autolock error).
any comment for this issue?
Below is the schematic…
Hi Adam, I understand what you want to check, I wish I had the equipment to provide the data. Working on that though... Meanwhile lets check the timing diagrams in PCM2706 vs TAS5713 datasheet.
Bytheway, the incorrect I2C address is explained here,…
Part Number: TAS5713 Other Parts Discussed in Thread: PCM2706
Hi,
In order to validate I2S and I2C communication in my application, I would like to make a quick&dirty setup similar to the TAS5713EVM, however without the amplifier output-filter and preferrably…
Part Number: TAS5713 I have a customer looking to use the TAS5713. They likely want to set up multiple equalizer settings. Please let me know if there is an easier way to program this part as opposed to generating many header files and putting all this into…
Part Number: TAS5713
I need to use the DRC in my current project. Like most TAS5713 registers, the documentation is not only insufficient, but that which exists is self-contradictory.
The DRC section of the datasheet at http://www.ti.com/lit/ds/symlink…
Part Number: TAS5713 HI
We are using TAS5713 DRC function and encountered a problem that left channel we can successful limit the output power at 27W however right channel the DRC fail to limit the output power.
My registor setting as below, may i have…
Part Number: TAS5713 Other Parts Discussed in Thread: TAS5733L , A few questions I'd like to be sure of...
1. The datasheet specifies registers 40 and 43 as 8 bytes. However, the GUI tool generates 4-byte values for these locations. I'm unsure why it…
Part Number: CC8530 Other Parts Discussed in Thread: TAS5713 , TAS3251 , TAS2562 CC853x support,
Our customer is starting a design with CC8530 sending audio to TAS3251. They need to configure the TAS3251 and adjust volume levels on the fly. The TAS3251…