Part Number: TAS5731EVM Hi team,
A customer need this EVM 's design files base upon EDA software not PDF.
Can you provide them?
Altium Designer format is more better.
you can also send them to my email.
X1054259@ti.com
Thanks.
Part Number: TAS5731EVM Dears
TAS5731EVM (TAS5731 power amplifier + tas57xxpsia) why connect the computer, the display driver error, the upper computer board unchanged, replaced by (MC57xxPSIA+ tas5711 power amplifier) is ok, I would like to ask how this…
Part Number: TAS5731M Other Parts Discussed in Thread: TAS5731 Hi
We have two TAS5731EVM board, But now they can't be identificated by the computer. We doubt the driver for TAS5731 is lose. Can you share the driver for TAS5731EVM ? thanks
Part Number: TAS5731EVM Hi team,
Customer use MC57xxPSIA in TAS5731EVM to write I2C to their own board, but have some issue in connection, here is the situation:
They disconnected the 5731EVM and flywired 3 wires from MC57xxPSIA to their own board, for…
Part Number: TAS5731EVM
Hi Team, Cusotmer is asking for the TAS5731 EVM OTP output power under the following the conditions. I do not have the EVM on hand. Would you please let us know what the OTP result is? (even the THD is >10%)
1) For 1.0 PBTL 24V…
Part Number: TAS5731EVM I am using the amplifier in 2.1 mode and have confirmed via adjusting individual volume settings in the GDE that each channel is being correctly routed to the correct speaker driver.
The problem is that when setting a high-pass…
Part Number: TAS5731EVM Hi,
I need some help to see if the speaker spec, below can be used along with TAS5731EVM.
Earlier we were using totally 3 speakers shown in below link
http://www.mouser.com/ds/2/334/AS06004PS-R-982169.pdf
Connections are shown…
Part Number: TAS5731EVM Hi,
I have a question regarding the TAS5731M amplifier.
When I do not have the amplifier without any charge, I can see that the coils are getting quite hot, a symptom that current is passing through them but I do not understand…