Hi Wei
Wei Qiu said: When this problem occurs, it will fail no matter how many times you send to the address?
When I tried set 0x00 and 0x01 alternately for subaddress 0x04(Left Channel Volume Control), I2C errors(return NACK) occurred approximately 50…
Part Number: TAS5760L Hi All,
I am using ESP32 in a prototype, along with the TI TAS5760L. The I2C bus is working and I can read and write to the registers.
Presently, I get the following outputs from the registers:
Register Values Amplifier Disabled…
Part Number: TAS5760L Dear Team,
I have a question about Soft Clipper of TAS5760L. Is the behavior of set "Resistor to GVDD" to (Open), same as set "Resistor to GVDD" to 0Ω? I'd like to ask wheather I can disactivate the use of…
Part Number: TAS5760L We are using an TAS5760L with MCLK connected to SCLK and ratio of SCLK/LRCK 64. But we get no audio at all. I found a post from 2017 where this very issue is addressed, but the datasheet still says it should support 64x. I'm a little…
Part Number: TAS5760MD Other Parts Discussed in Thread: TAS5760M , TAS5760L Hi, Team
In one of the MP project(PCB fix), Our customer use TAS5760 M, the pin18-31 NC pin connect to GND, that is match our datasheet. (they didn't use headphone function in this…
Part Number: TAS5760L Tool/software: Linux Hi there,
I evaluated the TAS5760L through the evaluation board, then I designed my audio circuitry with this part.
During the verification, we successfully talked to the part through the I2C connection, then…
Part Number: TAS5760L Other Parts Discussed in Thread: TAS5760M Dear Sirs,
My customer asked us about output voltage level of TAS5760L at THD+N≦0.8%. When he checked on his prototype board, the output voltage was 6.8 Vrms (7.9 W). So he was asked whether…
Part Number: TAS5760L Hello
Customer would like to know how may EQ can tuning for smart amp ? what is min. tuning +-dB? Could EQ tuning total audio band range ex 10Hz~20Hz ? Thank you.
BR
Patrick
Part Number: TAS5760L Hi team,
My customer follow the sequence as the datasheet.
But there is some sharp sound when they pull high and pull low the SPK_SD pin.
So we suspect it's because there may need a delay between pull SPK_SD and unmute channel,…