Part Number: TAS6424M-Q1 Hi TI
The customer found the following abnormal phenomena during testing TAS6424M-Q1:
The TAS6424M-Q1 driver does not have any abnormalities with speakers without a frequency divider, but there is a probability that speakers…
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 , TAS6424E We are considering using the TAS6424M-Q1 in PBTL mode with a 1ohm load.
We refer to "Figure 82. TAS6424M-Q1 Typical 2-Channel PBTL Application Schematic" in the Datasheet.…
Part Number: TAS6424MS-Q1 Other Parts Discussed in Thread: TAS6424E-Q1 , TAS6424MS Hi team,
My customer is asking if TAS6424MS-Q1 supports spread spectrum.
I can see it supports on TAS6424E-Q1; however, i cannot find it on MS datasheet (slose66).
Can you…
Part Number: TAS6424MS-Q1 Please check the Rjc(top) is 0.4°C/W or 0.7°C/W of TAS6424MS-Q1.
It's 0.4°C/W in 7.4 Thermal Information but 0.7°C/W in Table 12-1 of tis Datasheet.
Thank you
Part Number: TAS6424M-Q1 Hello team
I want to ask the question for TAS6424M-Q1.
When we use it in PBTL mode, what is the impedance of the speaker that we can diagnose?
In datasheet, the minimum speaker impedance of TAS6424M-Q1 is 1 ohm in PBTL mode…
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 Hello members
I want to ask typical latency in TAS6424*-Q1 series.
I understand that max sample count is 30.
How many typical counts in TAS6424?
I have checked below thread but there is…
Part Number: TAS6424M-Q1 Now I'm calculating the ripple current of the output inductor. Is the idle state ripple current the maximum ripple current that flows through the inductor.
Part Number: TAS6424M-Q1 Other Parts Discussed in Thread: TAS6424 Hi,
I want find I2S HUB(1 to 2) and can support TDM function,
is there have better solution except TAS6424M?
Thanks!
Part Number: TAS6424M-Q1 Hello,
When TDM data is input, the device automatically selects TDM mode. Is this only the case when "SAP Control (Serial Audio-Port Control) Register (address = 0x03)" is its default setting? My customer is experiencing difficulty…