Part Number: TCA6408A Hello,
I noticed in the TCA6408A manual (ver. SCPS192E) on page 3 that it is recommended to connect the ADDR pin directly to VCCP or GND.
However, in the layout example on page 33, the ADDR pin is connected to VCCI.
If I am using…
Part Number: TCA6408A-Q1 Other Parts Discussed in Thread: TCA9539-Q1 , Hi team,
My customer uses two TCA9539-Q1 in their system, which gives them 32 external GPIOs. However, they still need 4 other GPIOs to control CAN device. So they want to use TCA6408A…
Part Number: TCA6408A-Q1 Dear TI experts,
My customer made their first schematic with TCA6408A-Q1. Could you review the schematic below?
Best regards,
Chase
Part Number: TCA6408A Other Parts Discussed in Thread: TCAL6408 Hi there,
I've used TCA6408A before and the I2c bus will be stuck during high temp if VCCI is powered before VCCP, also TI has provided a new package to address this issue. May I know…
Part Number: TCA6408A Other Parts Discussed in Thread: TCA6408 Could you please provide me the DTS for TCA6408ARSVR evaluation? DTS is requested from the software development team.
Part Number: TCA6408A I have a design where VCCi will be +3.3V and VCCp will be +1.8V. Often, VCCp will be unpowered, and the peripheral connected to the GPIO ports connected to VCCp will be unpowered. VCCi will be powered, and there are other peripherals…
Part Number: TCA6408A Other Parts Discussed in Thread: TCA6416A Hello guys,
One of my customers received PCN of TCA6408A and TCA6416A recently. Also each device datasheet versions are changed from SCPS192D to SCPS192E for TCA6408A and from SCPS194E to…
Part Number: TCA6408A Hi Team,
On my design (P5-P7) are not used. I am not sure D/S coves the case parallel pin is not connected and left open.
Is that Okay or PU/PD should be added?
best regards.
Part Number: TCA6408A-Q1 I have some concern regarding with i/o Expander TCA6408AQPWRQ1 INT Pin.
Now, I want to add above 2 Switch on GPIO as input with this Expander IC and connect it with this Deserializer. for same i have some questions.
Q1. At which…