Part Number: TCAN1042-Q1 Hi Team,
Could you please kindly help to check for TCAN1042 terminal resistor as below R7 and R15 shows, why a 0805 package size resistor is needed here? What would be the maximum power through these resistor? Thanks a lot for…
Part Number: TCAN1042-Q1 Dear TI experts,
My customer asked the location of resistors in communication line. Could you check that which one is right for case 1 and case 2?
Case1) 250Kbps communication speed.
1-1. 120ohm resistors are located in the start…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , Hi team,
My customer uses TCAN1042DRQ1 in their project. And they met below question, could you please help give some comments? Thank you!
For the TX dominant timeout feature of the…
Part Number: TCAN1042-Q1 Dear TI expert,
Our product uses TCAN1042-Q1 as the CAN transceiver, we found a problem during the test, after the 1042 is awakened, it will continue to output a low level of 2ms, which causes the receiver device to continue to…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1057A-Q1 , TCAN1044A-Q1 , TCAN1057-Q1 , Hi Expert,
Customer would like to do the compatible design between TCAN1042 and TCAN1057. Would like to check with you if PIN5 NC of TCAN1042 can connect…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , Hi,
Dose tcan1042 support hot plug? By hot plug, I mean two already powered up devices connect CANBUS with cable.
Part Number: TCAN1042-Q1 Hi
could you help to suggest suitable products Thank you
CAN FD Transceiver : Bit rate Up to 8Mbit/s ( 5Mbit/s also available )
CAN XL Transceiver
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: TCAN1044A-Q1 , , TCAN1042V-Q1 Hi expert,
Customer used TCAN1042 and test FMA for CHAH&CANL short to VCC. Requirement shall be minimum class C according to the ISO16750.
From the spec showing…