Part Number: TCAN1042GV-Q1
I AM NOT ABLE TO FIND THE DETAILS OF THE ABOVE BODY MARKING DETAILS IN THE DATASHEET PLEASE COME BACK WITH DETAILS [TCAN1042VDQ1]
Part Number: TCAN1042GV-Q1 Hi Team,
The customer can measure waveforms in CANH and CANL, but no signal is detected in TXD and RXD. Could you please help with the analysis? Please help to review the schematic below. Thanks.
Regards,
Hailiang
Part Number: TCAN1042GV-Q1 Hi,
Can I avoid using external ESD protection circuitry while using TCAN1042GV-Q1 CAN IC as it has got internal protection up to +/-16kV.
Regards,
Sunney
Part Number: TCAN1042GV-Q1 Hello,
Please can you confirm if it is OK for the exposed pad on the DRB0008F (i.e. VSON) package to be connected to GND (i.e. connect to the same GND net as pin #2)?
I have searched through the current datasheet (SLLSES9C …
Part Number: TCAN1042GV-Q1 Hi team,
I'd like to confirm if our TCAN1042 can support off board TX and RX connection? For example, we have LED driver on one board and TCAN1042 on another board, we want to connect the TX and RX by wire about 10cm~20cm. Is…
Part Number: TCAN1042GV-Q1 Hi,
What does the product marking for these two mean?
This was not described in the datasheet, if it's documented somewhere else, please guide me. I'm looking for the meaning of each character.
Thanks, Fredrik
Part Number: TCAN1042GV-Q1 Hello,
Please can you confirm if it is OK for the exposed pad on the DRB0008F (i.e. VSON) package to be connected to GND (i.e. connect to the same GND net as pin #2)?
I have searched through the current datasheet (SLLSES9C …
Part Number: TCAN1042GV-Q1 Dear TRX expert,
My customer is using TCAN1042GVDRBRQ1 and schematic is shown as below:
The STB is connect to GND through a 10k ohm resistor, and VIO is connect to 3.3v supply.
The question is, Will the internal source at STB…