Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042H Hi Team,
Please share the +-70V bus fault test report of TCAN1042H. My customer would like to check it. Thanks.
Regards,
Alex
Part Number: TCAN1042H-Q1 Other Parts Discussed in Thread: TCAN1042H Hi
May customer is not sure if they need 70V fault protection or not.
may i ask in which scenario may cause +/- 70 fault protection need for the CAN transceiver ?
and how do i check my…
Part Number: TCAN1042H-Q1
I see that 58V BUS voltage is sufficient in ISO 11898-2:2016(E) standard. What is the advantage of "TCAN1042HDRQ1" integrated with 70V BUS voltage?
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: DRV8353R VCC and Gnd pins of TCAN are found short when we removed IC out of board as it was not functioning.
Is there any specific root cause for such internal short?
We are using buck converter…
Part Number: TCAN1145-Q1 Other Parts Discussed in Thread: TCAN1042H TCAN1145-Q1, in normal operation, CANH and CANL will be burned out if short-circuited to 32V.
Thanks Clemens!
Hi Jie,
You can reference the thread linked below for more information on CAN termination resistor sizing: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/986855/tcan1042h-q1-the-power-rating-needed-for-the-termination…
Part Number: TCAN1042H-Q1 Hi
My customer are using TJA1042T with split circuit.
Can TCAN1042H-Q1 do drop in replacement for TJA1042T without PCB and BOM change ?
Like to make sure if TCAN1042H-Q1 can be used in this way or not ?
Part Number: TCAN1463-Q1 Other Parts Discussed in Thread: ISO1042 , , TCAN1044A-Q1 , TCAN1043H-Q1 , TCAN1042H-Q1 Hello,
My customer has some questions about the CAN interface isolation.
Q1. When CAN communication is connected as shown below, is there a solution…