Part Number: TDA3MV Hello
I want to scale up 640*480 to 1280*1024.
I used VXLIB.
I set it as below and DSP died.
what is the problem..?
/* scaleImage */
VXLIB_bufParams2D_t src_addr;
VXLIB_bufParams2D_t dst_addr;
src_addr.data_type = VXLI…
Part Number: TDA3MV Hello.
I used dss resizer or isp resizer to enlarge the image 4 times larger than the capture. (640*480 -> 1280*1024)
However, in both methods, the starting point is shifted as shown below, causing the video to shake.
How can I…
Part Number: TDA3MV Hello
Thanks for the reply below.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1279930/tda3mv-a-blinking-square-box-at-the-end-of-the-video
Is there a way to know if fill in all the buffer ?
Part Number: TDA3MV Hello
I'm using TDA3xMVS.
I set SBL_LIB_CONFIG_DSP_1000GHZ_EVE_900MHZ to 1u in sbl_lib_config_tda2xx.h.
Before entering the usecase, the frequency is as shown below.
However, when entering the usecase, the following error occurs…
Part Number: TDA3MV Hi
I have a problem about a blinking square box at the end of the video.
It works fine at 30hz, but there is a problem at 60hz.
And in number 1 below, a square box appears, but in number 2, it operates normally at 60hz.
1 (Issue…
Part Number: TDA3MV Hi,
We are operating TDA3MV using 20MHz Clock.
To develop BT.1120 output, we want to change this clock from 20MHz to 27MHz (We think that making 74.25MHz in device needs 27MHz).
We first changed hardware (oscilllator device and resistor…
Part Number: TDA3MV Hi team,
Depending on the TDA3EVM to design the board, the following issues occur when running the program:
Here's the config message, could you help locate where this error occurred?
/home/cy/PROCESSOR_SDK_RADAR_03_08_00_00/vision_sdk…
Part Number: TDA3MV Dear Champs,
When customer removed osc1 in their custom board, they found below issues related with QSPI flash.
Is there any relation between SYS_CLK2(or osc1) and QSPI flash?
1. When qspiFlashWriter_m4)release.xem4 load & run to…
Part Number: TDA3MV dear
1. Does it support 1080P 60fps 4-camera input or 720P 60fps 4-camera input?
2. support video output 1080P 60FPS?
3. Does it support 3D viewing and transparent chassis display?
4. Does the system delay requirement of 60ms satisfy…