Can you clarify what product you are using? Keerthy has suggested some dip switch settings which are used on the EVM. However, you are stating the SOM is soldered - so I'm not clear on which product you have. What is the "TDA4VMXEVM-BUNDLE"?…
Hello, TI members.
After the software migration from PSDK 7.1 to PSDK 7.3, two kinds of issues started to occur.
These errors occurred during aging testing and I've never seen these errors in previous PSDK versions.
- ti-processor-sdk-linux-j7-evm…
Part Number: TDA4VMXEVM Hi,
at
at "Hardware Setup Details": You are refering to a special cable from adexelec.com. Could you please share a direct link / part number to that cable which is required?
Best Regards, Thomas
Hi,
Ionut Cretu said: We see that Can_Write is executed but we don't see any frame that are send. In Can configuration we use MCU_MCAN0 and we use the Can_0_Int0ISR interrupt.
1. Is the ISR getting getting triggered?
2. Is the setting on the PCAN correct…
Part Number: TDA4VMXEVM Hi TI expert,
On the TDA4 EVM board, I run my own test code to test the UDMA memory to memory transmission(TR descriptor). The test code will allocate a DMA channel to move the source memory filled by test data to the target memory…
Part Number: TDA4VM
Hello.
Flow Vector Output Data Packing Format
Horizontal flow vector (9bit signed integer, 4 bit fractional):
[19:16] Fractional is 4 bits (support 1/16th pixel of precision)
[28:20] Signed Integer is 9 bits (support up to +255…
Part Number: TDA4VH-Q1 Hi team,
In our custom board we have UFS(MTFC128GBCAYAL-AAT) Flash memory. So I have doubt that for provisioning the UFS controller for first time is the 5554.5758.config_desc_data_ind_0.7z is enough or we need to do some modification…
Hi, TI members
I have a camera running to 60FPS.
So, the graph is also processed to 60 FPS. But I want to change it to 30FPS.
I would like to know if there is a way to change the graph to be processed to 30 FPS.
For example, one frame is processed and…
Part Number: TDA4VMXEVM Hello TI team
I tried to order TDA4VMXEVM-BUNDLE but it says "it does not exist".
I'm thinking to order J721EXSOMG01EVM and J721EXCP01EVM separately.
is there any difference to order separately or BUNDLE set?
thank…
Part Number: TDA4VMXEVM As I do not have SD card,i want to boot TDA4EVM by u disk
But I only find SD card boot introduce in Processor SDK RTOS Automotive 06_02_00,nothing about USB boot
There are document about USB boot for me,Thanks