Part Number: TDA4VMXEVM Hi
I've been looking up some information about TDA4VMXEVM.
Now I'm curious about profiling SDK on that SoC chip with running Linux.
If there is not, then can I use any profiling tools such as timemory, Vtune?
Actually,…
Part Number: TDA4VM Problem (or) Issue: TDA4x: No LIVE Streaming from TDA4 + IMX390 with prebuilt vision apps
Is there specify display(monitor) we have to use for live streaming? Also is there specify connection (say DP only) to use?
My setup: I am…
Part Number: TDA4VMXEVM Hi,
I am trying to remove unwanted packages from yocto build
for example i don't need bridge-utils in my build
cd ti-processor-sdk-linux-automotive-j7-evm-07_00_01/yocto-build/build
vi conf/local.conf
at the end of the file…
Hi, TI members
I performed a video encoder processing test according to TI user guide.
As you can see below, a timeout error occurred once at first time during the conformance test.
[MCU2_1] 3931.060951 s: TIMEOUT: topazdd_wait_on_sync timed out waiting…
Part Number: TDA4VMXEVM Hi,
Copy SBL binary sbl_mmcsd_img_mcu1_0_release.tiimage as tiboot3.bin
Copy the sysfw.bin form ($PSDKRA_INSTALL_PATH)/(pdk-install-folder)/packages/ti/drv/sciclient/soc/V1/sysfw.bin as sysfw.bin
Copy the application from ($PSDKRA_INSTALL_PATH…
Part Number: TDA4VMXEVM Hi,
After having installed, built, setup EVM and SD card for vision_apps,I fail to run the demos.And the errors are shown as below.Can you help me solve it?
root@j7-evm:/opt/vision_apps# ./vx_app_tutorial.out APP: Init ... !!! APP_LOG…
Part Number: TDA4VMXEVM Hi,
1. Is there any kind of mechanism in the TD4VM/DRA829Vx hardware or in the LINUX_SDK which handles frame rate variation on CSI-2 video input stream? Namely, what if the video is suddenly cut off for some time, for example,…
Part Number: TDA4VMXEVM Hello
I am currently working on TDA4 along with the EVM (common processor board). I am trying to run the initial setup demo (Jacinto 7 EVM Quick start guide). Link to the demo : www.ti.com/.../spruis8.pdf
I had followed the steps…
Part Number: TDA4VMXEVM Hi,
I following the user guide under “psdk_rtos_auto_j7_07_00_00_11/psdk_rtos_auto/docs/user_guide/developer_notes_sbl_boot.html?highlight=boot” to compile the SBL.
The first step that I’ve done is to launch the command…