Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 , MSP430FR6043 , TDC7200 Hello all, I have a question.
I would like to use a TDC1000-C2000EVM and two 2 MHz transducers to detect the flow rate of tap water flowing through a PVC pipe…
Part Number: TDC1000 Other Parts Discussed in Thread: TUSS4470 , PGA460 , Can this chip be used for level sensing on small fluid bottle 5.5 inch (140 mm) ?
Part Number: TDC7200 Other Parts Discussed in Thread: TDC1000 , , MSP430FR6047
Hello,
I'm working on a project to develop an ultrasonic flowmeter using the time of flight (TOF) method. I'm using 2 transducers (2 MHz), TDC1000 (AFE) and TDC7200. I am also…
Part Number: TDC1000 if we directly connect the received signal from transducer(avoiding LNA and PGA) to compin, directly do we have to place any filter inbetween LNAOUT and COMPIN,if yes which kind of filter can be used?
Part Number: TDC1000 Other Parts Discussed in Thread: PGA460 , TDC7200 , DRV8870 Hello,
I am trying to find a good solution to measure the depth of the water using an Airmar P19 depth transducer, which is mounted on a sailing boat, few cm under the floating…
Hello Isaac,
Thanks very much. Yes, the RTD interface is on the TDC1000. I wrote the configurations into the registers of TDC1000, and I got the START and STOP signals out from TDC1000 pins. Below listed the scope time of RTD measurement, and I think…
Part Number: TDC1000 Other Parts Discussed in Thread: MSP430FR6043 we are using TDC 1000 in our work, and we saw a driver circuit used in sample schematic which was there in Ti website.. could you please explain whether its necessary to use this driver…
Part Number: TDC1000 Other Parts Discussed in Thread: PGA460 The TDC datasheet says the measurement range is up to 8 ms for the TDC-1000 but I would like to increase that to 30 mS. Is that possible? I know I need to increased the excitation voltage which…
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 Is there any processing being done by the firmware or software on the displayed TOF values (From the start/stop pulse timings)? I've got the number of stop events set to unlimited,…