Part Number: TDC7201-ZAX-EVM Other Parts Discussed in Thread: MSP430F5529 , I have a TDC7201-ZAX-EVM which I attached to a MSP430F5529 Launch pad to test out. I used the LabView based GUI and followed the instructions with the TDC7201-ZAX-EVM on how to connect…
Part Number: TDC7201-ZAX-EVM Other Parts Discussed in Thread: LMG1020 , TDC7201 Hi there,
Application: laser rangefinder Demo Module using TDC7201-ZAX-EVM and LMG1020EVM
Question 1: how to connect a LIDAR START (or laser on) signal from LMG1020EVM board…
Part Number: TDC7201 Our client used TI's TDC7201 for the laser ranging project, and now they are encountering some problems. Do you have any solutions?
When using multiple TDC7021 chips, we found that some of them were OK, and those that were not…
Hello Chuanfu,
It looks like design has their resources tied at the moment so they are not able to look in depth into this. So I did some tests on a couple of units all at 3.3V and it seems like the threshold is about 1.71 for this Vdd level. This does…
Part Number: TDC7201 Other Parts Discussed in Thread: TLV3601 , Hi,
Customer question:
Is impedance matching required between the output of the comparator (TLV3601) and the input STOP2 pin of TDC7201?
Thanks,
Tyler
Part Number: TDC7201-ZAX-EVM I see a pot from three years ago saying example code is available in GUI install folder. I don't see it in there. Has it been removed or am I missing something?
Part Number: TDC7201-ZAX-EVM Other Parts Discussed in Thread: TDC7201 , , MSP430F5529 , MSP-EXP430F5529LP Per instructions on quick start guide I've flashed the MSP430 with TDC720x firmware. Had to complete this in Linux BASH because firmware update tool…
Part Number: TDC7201-ZAX-EVM Other Parts Discussed in Thread: TDC7201 , TDC7200 I'm trying to use the received signal from the HCSR04 ultrasonic sensor as a trigger for the TDC7201 and am controlling both using an arduino. While I can get an output from…