Other Parts Discussed in Thread: TFP501 , PCA9546A , PCA9548A TFP501 specification (http://www.ti.com/lit/ds/symlink/tfp501.pdf) seems to have described I2C Base address with read/write bit included.
Thus, the real TFP501 I2C Base address, in terms of I2C…
Hi Rick,
That document is for the TFP501/403, not for the TFP401.
In the TFP403 datasheet, the pin description for these pins says "Reserved. See TFP501 data sheet for intended future use."
In the TFP501 datasheet, these pins are in fact…
Hello Rick,
The ref schematic that you linked is for the TFP501/403. These are not the same as the TFP401A. The datasheet and ref schematic are both correct.
Regards,
I.K.
Hi Vincent,
Are you referring to the reference design of TFP501 instead? TFP401A doesn't use EEPRROM.
Can you send me the link to the reference schematic?
Regards,
Dennis
TI does not have a multi-format video decoder unfortunately.
The closest would be a TVP5150/TVP5147/TVP5160 for PAL/NTSC, a TVP7002 for analog RGB/YPbPr and a TFP401/TFP501 for DVI. We don't have HDMI or Display Port receivers.
BR,
Steve
Hello,
The TFP403 is only a de-serializer, the audio signal is transmitted during the blanking periods in which the DE signal is low, thus the QE[], QO[] outputs will be low.
The TFP403 does not support HDCP so the Video Source won't be able to establish…