Part Number: THS1209 Other Parts Discussed in Thread: MUX36S16 , , THS4131 , OPA2277 I am using THS1209 running at 5MHZ to interface with 128 sensors which is selected by mux36s16 one by one, the mux36s16 turn on frequency is 200kHZ. The interface between…
Part Number: THS1209 Dear team,
Customer want to know when they use THS1209, how about the connection of Pin 15(conv_clk), Pin 16(Sync) and CS1 with F28335? Directly to IO port?
Thanks.
Best regards,
Sammi
Part Number: THS1209 Other Parts Discussed in Thread: THS1206M-EVM , THS1206 Dear team,
Could you provide the EVM schematic of THS1209? Or other TI design schematic related about THS1209?
You could send to my email: a0223722@ti.com.Thanks.
Best regards…
Part Number: THS1209 I use the THS1209 in two-channel mode via a xilinx spartan6 FPGA. The problem is that the SYNC signal is not receiving properly. After initialization by writing 0x401, 0x400, 0x088 and 0x482 to the register, the SYNC signal is fixed…
Other Parts Discussed in Thread: THS1209 Hi Champs,
Q.1) My customer would like to use ths1209 with single conversion mode as below.
Is there any concern in this use case?
Best regards,
Nobuo Fujihara
Hi 5111212 ,
The power is the dual supply +-12V and the signal level is +-12V, I want to get 1/8 gain.
Enclosed is a circuit that will meet the above requirements.
OPA277 E2E 03162021.TSC
I have some questions. THS1209 is ADC with BW is 2MHz. But THS4131…