Part Number: THS3217 Other Parts Discussed in Thread: DAC3162 , Hello, engineers: I would like to ask a question. I am designing a circuit using DAC3162 and THS3217. I notice that the datasheet for the THS3217 labeled the input common-mode voltage range…
Part Number: THS3217 The product description can be enlarged 20 times, but the actual amplification can only be 2 times. Please help to confirm the problem
Part Number: THS3217 Hello E2E,
Our customer made an engineering board with the THS3217. After power on, the package of THS3217 get hot reach 60-deg. The output is open.(non-load)
Please let me know why the device gets hot?
I looked previous post on E2E…
Part Number: THS3217 Hi Team,
According to the datasheet the THS3217 can be operated from a single-sided 8V (or higher) supply, however all the datasheet specifications are for a split +/-6V supply. What sort of performance degradation might we expect…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 , , LMH3401EVM , BUF602 Hi Experts,
Good day. We have this query from client about THS3217:
In the D/S this part is written to interface with a DAC (current driven), but can we drive this part…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 , LMH6703 , OPA695 1) We are using the Diff amplifier PN: THS3217 and our maximum operating frequency up to 800 MHz’s We want 0dB gain for entire BW from DC to 800 MHz signals. We wanted to…
Part Number: THS3217 Other Parts Discussed in Thread: THS3215 Hi Team,
We have designed a DAC circuit with using THS3217 part. Our design requirement as below,
Bandwidth (-3dB) at least 10MHz
Support output range +-5V
Output drive current >=25mA
…
Part Number: THS3217 Hii,
OPS output gain is configured as 2.5 as per the datasheet table 2.
But we are not getting output 10Vpp as per the 2Vpp input in OPS section. As per the suggested value its not at all amplifying. Output is same in input we are…
Part Number: THS3217 Other Parts Discussed in Thread: THS3091 , THS3491 Team,
Please help to answer on customer query on previous e2e thread - https://e2e.ti.com/support/data-converters/f/73/t/839127
--------------------
Hi Rohit,
We thank for your support…
Part Number: THS3217 Other Parts Discussed in Thread: AFE7225 , THS4221 , THS3215 , THS3491 Hi Team,
We are designing a 2 channel DAC circuit using analogue front end AFE7225 part. The output of the DAC we are converting D2S by using THS3217 part and the…