Part Number: THS3217EVM Other Parts Discussed in Thread: THS3215EVM , , THS3217 Hello, engineers: I would like to ask a question, in the application THS3215EVM and THS3217EVM (SBOU161A), I see a lot of test points are not directly added to the trace, but…
Part Number: THS3217EVM Other Parts Discussed in Thread: OPA134 Hello
We are new to this board and are not sure of having read the manual properly. The issue is we get 4 mV or 40 mV when we use the OPS amplification even if the differential signal we want…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 , I ordered two THS3217 EVMs to prototype a DC-coupled DAC driver circuit for a Xilinx RFSoC driving an I/Q mixer. I would like to connect +VCC to 6V and -VCC to -6V. However, it appears that…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 , , LMH3401EVM , BUF602 Hi Experts,
Good day. We have this query from client about THS3217:
In the D/S this part is written to interface with a DAC (current driven), but can we drive this part…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 , LMH6703 , OPA695 1) We are using the Diff amplifier PN: THS3217 and our maximum operating frequency up to 800 MHz’s We want 0dB gain for entire BW from DC to 800 MHz signals. We wanted to…
Part Number: THS3217EVM Hi,
The manual states that this produce has a fixed 2 V/V gain. It would be useful for our application to increase that value by maybe a factor of 2 or 4 without adding any extra components.
Can the resistors on this board be reconfigured…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3217 Hi there,
Can I use THS3217 as a bias tee to add DC to a single-ended AWG output (e.g Vin+ for signal and Vin- for DC)? Our application prevents us from using conventional bias tee which…
Part Number: TAS2563 Other Parts Discussed in Thread: THS3217EVM , THS3215EVM
Hi Team, customer is evaluating TAS2563EVM. in d/s figure 49, it shows the differential to single ended filter(D2S). Could you please let me know how to order this board for…