Part Number: THS4503 Other Parts Discussed in Thread: ADS1675 , THS4130 , TINA-TI , THS4551 , THS4541 This probably applies to all the THS diff amp products.
I am using the amp as an ADC input with VCOM offset as well. I have a gain less than unity and I have…
Part Number: THS4503 Other Parts Discussed in Thread: THS4541 Hello,
How to set the Rf and Rg resistor of THS4503? I need to change the 1.0~2.3V input to each -0.05~1.95V output of THS4503, and the output common mode voltage is 0.95V for the ADC.
…
Part Number: THS4503 Hi team,
I refer to the application circuit of ths4503 and simulate it, but the simulation result is different from the theory
The frequency of my input signal is 25kHz, and the input signal is 0 ~ 4V
Please help me analyze it. Thank…
Part Number: THS4503 Other Parts Discussed in Thread: OPA627 , OPA656 , LMH6551 , THS4541 Hi team,
The voltage follower is constructed by OPA627, and then connected to THS4503 amplifier. It is correct to test the output of OPA627 separately. When the input…
Part Number: THS4503 Can the THS4503 be implemented without the thermal pad with grounded vias beneath it? Does that have any electrical significance or is it just used as a heat sink?
Part Number: THS4503-EP Other Parts Discussed in Thread: THS4503 , TINA-TI
Hi, I am trying to analyze a simple circuit using TINA TI for THS4503. I find some discrepancy in verifying the DC analysis by TINA TI versus the calculations using the equations…
Part Number: THS4503 Hi Team,
Customer is using this part and found Junction-to-board thermal resistance value is missing, can we have it ?
Thanks!
Andrew
Hello Sima,
first sorry for being late,
Thank you for your helpful notes, i'll give my comment in red one by one
1- "Looked into the waveform generator, and it has a voltage output between 38mVpp to 0.65Vpp with a max frequency of 12.5MHz with either…
Part Number: THS4503 Hi,
I used THS4503 in my board to convert a differential signal to a single ended one. I have used the same configuration as used in THS4503EVM, however, when no signal is connected the current consumption of THS4503 is almost 10…