Part Number: THS5671EVM I'm hoping to use the THS5671A to convert from an FPGA output to custom analog input board, but we are using single supply (+5V) for all our components. The DAC datasheet says it is specified for 5V analog supply as well as +/…
Part Number: THS3001 Other Parts Discussed in Thread: THS5671A , , LMH6723 , THS4271 , OPA695 , THS3215 , THS3217 , OPA837 I'm hoping to use the THS567EVM to convert from an FPGA output to custom analog input board, but we are using single supply (+5V) for…
Jim,
Thanks. I can confirm after a quick check that there is a synchronization pulse present on these two pins. This is good enough for me, I will jumper/solder to these pins and get my trigger. I would suggest sending this pulse to one of the SYNC outputs…