Part Number: THVD1550 Hello team,
My customer has some questions related with fail-safe function.
1. When /RE=H, fail-safe in THVD1550 doesn't work, right?
2. Are pin A and B pulled up to Vcc / down to GND in THVD1550, respectively?
Best regards…
Part Number: THVD1550 Other Parts Discussed in Thread: THVD1520 , SN65HVD3088E Hi team,
I have one question as I know SN65HVD3088 is an old part. I suggest THVD1550 to replace the competitor. SP485EEN.
Apart from ESD and speed, what are the differences…
Part Number: THVD1550 Other Parts Discussed in Thread: THVD1500 Hi,
I have related questions for THVD1550: Using THVD1550DR as alternate to DS3695AM/NOPB.
As per the suggestions i have used THVD1500 in the design. Which has signal rate of 500kbps. Then…
Part Number: THVD1550 Hello everybody.
I need to justify a requirement concerning its permanent behavior in the event of a short circuit of its outputs to 0V.
For me, this component limits its current to +/-250mA. it is powered by 5,3V.
This means…
Part Number: THVD1550 Other Parts Discussed in Thread: THVD1520 , , THVD1500 We have used DS3695AM/NOPB in our design. As we received PDN# 20230217002.3 saying DS3695AM/NOPB is discontinued and THVD1550DR is pin to pin alternate for this. We tried using…
Part Number: DS36277 Other Parts Discussed in Thread: THVD1550 , Hi team,
The web says that the DS36277 and THVD1550 are pin-to-pin, but it looks like the Driver Enable circuitry logic is different between the devices. Can you confirm that, in order to…
Part Number: THVD1550 Hi Teams,
Here are some questions about THVD1550.
1) from the data sheet it seems if the TX and RX were disabled together, it takes us to enable again. Is correct?
2) If the Re and DE were connect together. Ideally, the system will…
Part Number: THVD1550 Dear Specialists,
Regarding THVD1550, my customer has additional questions about Equivalent Input and Output Schematic Diagrams.
I would be grateful if you could advise.
---
In the attached document,
Please tell me about the part…