Part Number: THVD8000EVM Hi team,
my customer is currently evaluating THVD8000EVM. They have the following questions:
Some resistors are not populated, such as R8/R9/R10/R11. Why is that the case?
They would like to reduce the differential voltage (BA…
Part Number: THVD8000EVM Other Parts Discussed in Thread: THVD8000 Tool/software: WEBENCH® Design Tools Dear Sir,
We have completed the testing of 2 EVM Board of THVD 8000 and its working fine as per our application.I have some query while testing the…
Part Number: THVD8000EVM Other Parts Discussed in Thread: THVD8000 Tool/software: WEBENCH® Design Tools Dear Sir,
The THVD8000 RS-485 transceiver with OOK modulation for power line communication modulates data onto existing power lines. I have EVM board…
Part Number: THVD8000EVM Other Parts Discussed in Thread: THVD8000 Hi team,
please help with the below customer questions.
I was able to evaluate the boards yesterday. It seemed to work with no issues even at 2A for a short period of time. I have a…
The TIDA-00527 reference design has just low-pass filters between the bus lines and its supply rails, so it works only with 5 V. (Same on the THVD8000EVM.)
You would have to create your own board and insert a voltage regulator.
Hi Jacky,
I have added a few slide decks on the process behind this application as well as a schematic file.
One thing to note is that we didn't build a specific board when testing the application with the THS6222 + THVD8000 - we used already existing…
Hi Tom,
We have a new dedicated device that supports power-over-RS-485 that may interest you for this application: THVD8000. This is a 3.3V or 5V supplied RS-485 transceiver with built-in on-off keying that facilitates AC coupling a standard RS-485 signal…