Part Number: SOT23-UNIV-AMP-EVM Other Parts Discussed in Thread: LMV321-N I am confused about the frequency for the PWM signal coming in. It is between 0 and 3.3 V. The C1 and R1 form a low pass filter. Which I calculated to be 33 Hz, so I thought I''l…
Part Number: TAS5825MEVM Other Parts Discussed in Thread: TAS5822M Hi!
I am looking for a stereo power amp / speaker amp EVM that can take a digital audio input from a USB cable, connected to a Linux PC.
Actually the purpose of the stereo amp is to deliver…
Part Number: PLABS-SAR-EVM-PDK I acquired this evaluation module a few years back. Due to a medical emergency (my wife suffered a dual brain bleed) I shelved the EVM waiting for a time I could use it. Now at Lisa is doing much better, I set the module…
Part Number: LM5156 Other Parts Discussed in Thread: LM5155EVM-BST ,
for EVM: LM5156EVM-BST, or LM5155EVM-BST PCB, :
What is the total thickness ?
What is the thickness for each layer ?
TI Precision Labs - Op Amps www.ti.com/.../ti-precision-labs-op-amps.html
Stability - 3 and Stability - 6
How are these equations Aol_loaded and 1/β derived?
Part Number: SK-TDA4VM 1. Download ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05-Linux-x86-Install.bin and install. 2. execute sudo ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05/bin/create-sdcard.sh, create SD rd with prebuilt Image in the sdk …
Part Number: AWR6843 Hi Team,
We saw the Sprious at 57.6GH on AWR6843 on TI EVM. It is not acceptable for Japanese radio law.
Is this problem will be fixed for next gen like a AWRL6843?
Best regards,
Ito
YiFong Lin said: 1. source environment-setup
2. arm-oe-linux-gnueabi-gcc $CFLAGS helloworld.c -o helloworld
or
3. $CC helloworld.c -o helloworld -mfpu=neon -mfloat-abi=hard
For reference, the best/cleanest way is probably a combination of both approaches…