Part Number: TPS272C45 Hello,
I would like to save ADCs and would like to connecto more than on TPS272C45 SNS pin (over resistor, diode...) to same sensing resitor.
Is it possible?
Best regards, Miroslav
Part Number: TI-PLC-PRIME-SN Hello Errol,
I kindly request the requirements to change from PRIME v1.3 to PRIME v1.4. what are the main hardware differences from PRIME v1.3?
Kind Regards!
Behailu.
Part Number: TMS320F280025 Other Parts Discussed in Thread: TMS320F28035
Team,
I know that the TI-PLC-PLCLITE is not anymore made available. However:
Is it technically possible to have TI-PLC-PLCLITE (just the Lite version, not G3/PRIME) running on F28002x…
Part Number: TI-PLC-G3-CENELEC-SN Hello,
I search the SDK package TI-PLC-G3-CENELEC-SN-F28PLC84 for start point for study a system of light management using PLC technology.
I have request it in the TI web site but the answer is " TI no longer supports…
Part Number: TI-PLC-G3-DC Hi Support,
I would like to get the source code of TIDM-SOMPLC-G3-CENELEC, as a reference for my PLC Development Kit (LAUNCHXL-F280049C + BOOSTXL-AFE031-DF1).
Thanks,
Eric
Hi Pate,
Yes, I got the download links now. But there is a small question. It seems that the PLC-PRIME have two versions of SDK, one is TI-PLC-PRIME-SN-F28PLC84(VERSION 7.10.1.0), the other one is TI-PLC-PRIME-SN(VERSION 8.1.1.0) which is newer. The version…
Part Number: TI-PLC-G3-CENELEC-SN In the fire detection industry, analogue addressable systems use control panels and detectors (and devices such as interfaces) which communicate with each other by means of a protocol.
What protocol is this? Can anyone…
Part Number: TI-PLC-PRIME-DC Other Parts Discussed in Thread: AM3356
Can the upper level prime-dc v4.0.0.0 binary run on AM57x family with out an issue? Does it need to be recompiled for AM57x Family?
The below link describes that the upper levels of…
Part Number: TI-PLC-G3-CENELEC-SN Tool/software: Linux coordinator address has changed in response to the Discovery.request command. why?
i am developing G3 PLC service node. the coordinator address of the DC i used was 0x0000. 2 day ago the service node…