Hi Praveen,
I have query on similar lines. The page for TIDA-00011 ( www.ti.com/.../TIDA-00011) is very confusing. It says that the reference design use AFE4400 but in the 'Order Now' section link is given for AFE4403-HREVM. As you mentioned in this conversation…
Aleksandr,
Please try the code example contained in the TIDA-00011 OHRM health hub kit. It works with the MPU9150.
http://www.ti.com/tool/TIDA-00011
Regards,
Daniel
When I Bought the material for the TIDA-00011,I found that the "BR-LE4.0-S2A" bluetooth module cna't buy on the market.So I want to know if there is other bluetooth module i can used in the TIDA-00011? If there has, Could you Please tell me…
Lilli,
I'm sure this is possible and you might consider using our AFE44x0 devices. We have developed a few designs to help you get started, but please keep in mind this is for demo purposes only and TI is not an end equipment manufacturer. I have included…
Mike,
We do not have a proven design, but have lots of devices that you may be able to use. When developing a GSR device you want to measure a lot of biological things such as pulse rate, changes in muscle tension, skin temperature, respiration rate,…
Dear Mike,
Unfortunately we do not have any information related to this kind of technology. Chronos watch was design with other requirements/needs in mind.
Y can certainly use the following reference designs as a good starting point.
http://www.ti.com…
Inho,
We do not have a proven design, but have lots of devices that you may be able to use. When developing a GSR device you want to measure a lot of biological things such as pulse rate, changes in muscle tension, skin temperature, respiration rate…
Amy Ball's post of Sept. 29, 2013, mentions that some customers are using the AFE4400 for reflective pulse oximetry. I assume that means they are using the TIDA-00011 wrist unit, which contains the AFE4400 as front end, mounts the emitter and photo diodes…
TI Health Hub software that you have downloaded and installed, contains the firmwares for the Body Composition Monitor (TIDA-00008), Weight Scale with Body Composition Meter (TIDA-00009), Portable Pulse-Oximeter (TIDA-00010) and Optical Heart Rate Monitor…
Part Number: AFE4490SPO2EVM Other Parts Discussed in Thread: AFE4403EVM Hello,
I am trying to calculate blood oxygen (SpO 2 ) values given data output from the GUI. I am familiar with the equations:
R = (ACrms of Red / DC of Red) / (ACrms of IR / DC of IR…