Other Parts Discussed in Thread: TIDA-060001 , AFE031 Hi Team,
Our customer is looking for the TIDA-00067 documents. I have searched the forum but the files are not available. Can we have a copy?
Regards,
Danilo
Part Number: TIDA-00067 Hi,
We are intended to prove PLC communication between devices which is currenty RS 485 active on them.
I am looking for;
1) PLC on 48 VDC, but the DC will be changing 40V to 60V
2) Bit rate is 115200.
3) Transmission distance…
Part Number: TIDA-00067 Hello
I have a personal interest in DC Power Line Communication (PLC) over 12V (sailboats, they use normally 12V batteries). Do you know if it is feasible? Do you know of any previous attempt in 12V?
Thanks in advance!
Caio
Part Number: TIDA-00067 I search a power line communication solution for low voltage DC (24V or 48V) for a master thesis. Is it possible to buy the TIDA-00067 DC Power Line Communication (PLC) Reference Design?
Part Number: TIDA-00067 Champs,
I am asking this for customers.
They are looking for
1) PLC on 48 V DC, but the DC will be changing 40V to 60V
2) Bit rate is larger than 250 kbps
3) Transmission distance is about 1 meter
4) Support CAN input or…
Part Number: TIDA-00067 What is the actual current/power required for the PA of the AFE031 in the TIDA-00067 design/test? We are working on the same application, PLC over DC power line and are using the AFE031 on the both ends. In the TIDA-00067 design…
Can the PLC Reference Design TIDA-00067 be modified to transmit at data rates ≥ 10Mbps?
Can this design be modified to work at higher voltages?
What is the minimum SNR for this design? The DC power line for this application is somewhat noisy.
Other Parts Discussed in Thread: AFE031 Is there a functional reason (as opposed to a choice of target market) why the TIDA-00067 DC (24 V, nominal) Power-Line Communication reference design specs 18 to 35 VDC? With appropriate internal power converters…
Part Number: TMS320F28069 Other Parts Discussed in Thread: C2000WARE Tool/software: Code Composer Studio hi,
We are searching for a solution for Power Line Communication(PLC). we hope two nodes can communicate on a DC Bus Line, the DC voltage is about…
Vincenzo, hello. The literature number that you provided is associated to a very old TI Reference Design (TIDA-00067), which has been obsoleted. I will send you a copy of the old guide via email offline from this forum.
Best Regards,
John Fullilove …