Part Number: TIDA-00142 hello my question is it possible to run a bldc directly form the TIDA-00142 without using gui (without a pc) using just the potentiometer and start/stop buttons thanks for your concern
Part Number: Hello,
I need to design a motor controller for a 24 VDC / 250 Amp BLDC.for electric-powered hydraulic steering-assist pump.
There are different techniques:
1- with Hall-Effect sensors
2- Sensor-less BEMF zero-crossing detection
3- Sensor…
Part Number: TIDA-00142 This product is looking like it will fulfill the needs of our requirement, but do you have some guidance for implementing current feedback control and commanding this via the CAN bus? This will be used for an automotive prototype…
Other Parts Discussed in Thread: DRV8301 , CONTROLSUITE Hey Guys,
i want to run a 1kW BLDC-Motor with the TIDA-00142. There will float a max. current of 60A.
Don´t geht the MOSFETs too hot? Should i cool them down? I was wandering, because there is no cooling…
Hi Artin, First off, note that the TIDA-00142 works off the DRV8301-HC-C2-KIT baseboard. More information on that board can be found in controlSUITE (once installed) at the below: \controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\ What type of specs…
Isolation University.xlsx
Matthew,
I have attempted to include an excel sheet from the Isolation Department's ISO University. It contains several links to collateral explaining isolation and it's applications. If the attachment failed, type "iso/" in…