Part Number: TIDA-00164 Good morning I'm an italian engineer and I'm developing a data acquisition system for a company that manages waste water plants. My need is to acquire data from analog sensors and your ads8688 ADC seems good for my application…
Part Number: TIDA-00164 Hi there:
My customer would like to double check the 6V_ISO & 18V_ISO whether will over the spec of transformer (T1), they since like find the SEC side 5V/100mA ( https://katalog.we-online.de/ctm/datasheet/750342178.pdf ) notification…
Part Number: TIDA-00164 Hi,
I just would like to know what is the communication protocol between with PLC and TIDA-00164? (such as profibus, modbus ?)
Could you please refer to some documents?
Best Regards,
Mehmet
Part Number: TIDA-00164 Hello My purpose is to develop the tida-00164 board. From your database I downloaded two files. I downloaded the first file "tidu365b.pdf" (i.e. File_1) from link www.ti.com/.../getliterature.tsp and the second file …
Part Number: TIDA-00164 Dear Specialists,
My customer is considering TIDA-00164 and has a question.
I would be grateful if you advise.
---
According to TIDA-00164, 10M ohm resistor(R74) is connected in front of ADC8688.
What is the purpose?
Why is connected…
Part Number: TIDA-00164 Dear Specialists,
My customer is interested in TIDA-00164(tidu365b) and has a question.
Could you please advise in detail?
----Question
(1) What purpose is C12 of ADC input circuit?
Does this capacitor consist RC filter with R4…
Part Number: TIDA-00164 Dear Specialists,
My customer is considering TIDA-00163 and has a question.
Could you please advise?
---Question
I am considering Surge protection circuit.
According to the application note TIDA365B at P.9 Table 7 Ztotal,
Ztotal…
Part Number: ADS8688 The TIDA-00164 16-Bit, 8 Channel, Integrated Analog Input module for Programmable Logic Controllers (PLC) Reference Design employs Johanson Dielectrics P/N 202R18W102KV4E ceramic caps for use as "Y-caps". These devices are not rated…
Other Parts Discussed in Thread: ADS8684 Hi,
My customer Leadshine wants to use ADS8684 or 8688 on one PLC project.
In the TIDA-00164 user guide, there only has input voltage test report, but not input current report.
customer wants to know if we can provide…
Hi TTG,
I have got the confirmation, the reference design TIDA-00164 including TIDU365B documentation has been removed from the web and obsoleted. Thanks for your attention.
Best regards,
Dale