Other Parts Discussed in Thread: AMC1304M25 , AMC1304M05 , TMS320F28377D Hello there,
We are checking the above isolated current shunt and voltage measurement reference design based on AMC1304M05 and AMC1304M25 and we have the following doubts:
1. The design…
Hello Rajesh,
Please note that the isolation amplifiers have a +/- 250mV input.
Please refer to the below for delta measurement.
https://www.ti.com/tool/TIDA-00171
Regards,
Sreenivasa
Part Number: AMC1305M25 Other Parts Discussed in Thread: TIDA-00171 , Hi Sir :
I want to know
1.AMC1305 the Fclk =20Mhz is OK?
2.when input Vpp =0 the Dout = 0101 and sometimes It will be 1100 but AD7403 it just Dout 0101. I want to know why?
3.TIDA…
Part Number: TIDA-00915 Other Parts Discussed in Thread: DRV421 , INA253EVM , , TIDA-00366 , TIDA-00171 , AMC1311 , TIDA-00914 , AMC1301 , INA253 Dear Martin
We found two EVMs that we think can help us testing these daughter boards (LMG3411-18) in closed loop…
Other Parts Discussed in Thread: TIDA-00209 , TIDA-00171 , SYSBIOSSDK-IND-SITARA , SYSBIOS Hellow,
We are developing a Motor driver using the TIDA-00209.
We cann't find the AM437x firmware for the TIDA-00209, only find the TIDA-00171 firmware.
But it…
Hello Achref,
I will look into the 50mA operation, but I would overall not recommend using the INA250 with 55A peak load currents for the following reasons:
1. We cannot guarantee our specifications for 55A loads currents because we specify the absolute…
Hello Oliver,
Sorry for the delay in my reply.
The AMC1304M25 and AMC1305M25 are isolated delta-sigma modulators. TI’s delta sigma modulators are indeed listed as 20 MSPS ADCs (and 10 MSPS in some cases) due to the framework in which the devices are classified…