Part Number: TIDA-00239 Hi,in reference design 'TIDA-00239', there are Transformer 'T2,T3' used for DC/DC converter,. The Manufacturer PartNumber of T2,T3 is 750311492, but I can not find these two transformers on Wurth Elektronik website…
Part Number: TIDA-00239 Hello
I have a query regading current direction. Assuming that above design can be tweaked for active cell balncing with cell to module topology.Let's say we are charging a 14s1p battery pack and cell 6 is overcharged. So,…
Hi Mark,
If you are referring to the next version of the board, TIDA-00817 is on the TI web site, which describes a 16-channel active cell balancing solution, also known as EM1402. I am working on getting it released as an orderable item.
Regards,
…
Hi Steven,
TIDA-00239 provides a test report and design information of the EM1401EVM solution.
The EM1401EVM has a MCU on the board, and so it could be programmed as you wish, including an SoC algorithm. Unfortunately, TI cannot provide the source code…
Hi,
My customer will make board based on TI Designs.
They downloaded TIDA-00239 CAD Files and TIDA-00239 Gerber .
They tried to make the board, but they could not make a board because there is no drill data.
Can I get the data of dril center such as .drl, .lst…
Part Number: TIDA-00817 I am working on a Battery management system for a high voltage Li-NMC battery pack with the maximum pack voltage of 270VDC and a maximum capacity of 25Ah (8p32s). I was planning to implement the active balancing reference design…
Hi Naga,
Please message me - I have a couple preliminary app notes that may be helpful for you while designing. Off of the top of my head, I think it should be a fairly simple conversion to balance cells back to the module. We have a TI reference design…
Hi Lina,
The converter must be able to move energy between a cell and another supply, the EM1402EVM uses the external isolated 12V battery for this purpose, but you can use the module voltage instead. TIDA-00239 is an example of active balancing which…
Hi Che,
The EMB1499Q/EMB1428Q chipset describe what you are looking for. Together they make up an isolated DC-DC solution. You may study the EM1402 EVM, TIDA-00817, TIDA - 00239, and the EM1401 EVM.
The bq76pl455A and the EMB chipset can do module…