Other Parts Discussed in Thread: TIDA-00261 , BOOST-DRV8711 I would like to know if it is possible to use TIDA-00261 with the BeagleBone Black. Or if you have a similar product but it is configurable and manageable by sending strings.
Laura,
Thanks for considering our devices.
Yes the CSD88537ND is a good device for motor control. There are 3 motor reference designs on TI.com using this device,
Ref Design Number
Description
TIDA-00196
12V and 24V Brushless DC Outrunner Motor…
Part Number: BOOST-DRV8711 I have a TIDA-00261-BOOST-DRV8711 evaluation board that I am trying to see if the components are sufficient to operate the attached stepper motor. Without too many tweaks in the settings I could operate the motor but the motor…
Hello Andres,
Unfortunately, I don't believe that either of the boosterpacks that you mentioned will work for your application.
The BOOSTXL-ULN2003 is meant for simple, relatively low current (500mA max) stepper motor driving applications, and the…