Part Number: TIDA-00285 Tool/software: Code Composer Studio We're spinning a new version of the TIDA-00285.
We're having issues when trying to perform the motor detection.
Ideally we would like some code to run a open loop space vector modulation…
i am not able to find the "(tida 00285) 1-kW/36-V Power Stage for Brushless Motor in Battery Powered Garden and Power Tool" on the TI website but it was present earlier.
when i search the result show the given below. please send me the all…
Part Number: DRV8303 Dear TI expert,
I was using DRV8303 to drive a high speed PMSM with low inductance recently. The supply voltage is 28V. The drive board circuits is designed according to the TIDA-00285 design. The board could work at first. However…
Hello Pragash,
Winding voltage are typically sensed with a voltage divider and small RC filter that feed a uC or analog control.
TIDA-00285 is an example.
www.ti.com/.../TIDA-00285
On the schematic page 5 in the upper left are the dividers used to interface…
I would like to keep this one for a re-spin of TIDA-00285.
Vin = 15-50V
Vout = 12V @ 100mA
Seems like the parametric search tool has some specs, are these accurate?
Hello Sagar,
An example of a 1 kW design using our DRV8303 is attached below. This would be a good starting point for some of your quesitons.
www.ti.com/.../TIDA-00285
Hi Kai,
The reference design linked below is for a 36V, 1kW design using the DRV8303:
www.ti.com/.../TIDA-00285
I believe the reference design you're referring to is the 24V, 100W/30W design. The MOSFETs used in this design would not be rated for…
Part Number: TMS320F28027F Other Parts Discussed in Thread: CONTROLSUITE , Hi Colleagues,
I'm designing an EVM for motor control. Currently we are basing our design on the TIDA-00285 software.
My question: The motor control stuff expects the measurements…
1. Follow the TIDA-00285 design guide to setup the board, to ensure the power supply of board works well first.
2. As the chapter 7 design guide, it is compatible with "boostxldrv8301_revB" hardware and has the same pin configurations. You can use the…
Part Number: DRV8303 Other Parts Discussed in Thread: INA181 , Tool/software: Code Composer Studio I'm having an issue with a motor controller solution.
We started with TIDA design 00285 and replaced the internal current sense from the DRV8303 with…