Part Number: TIDA-00299 Other Parts Discussed in Thread: TMDXICE110 , TMDSICE3359 , AMIC110 , AM3359
Dear distinguished engineer,
I migrated ecat_appl project code from TMDSICE3359 to TMDXICE110, after loading this ecat_appl.out file, it mentioned error…
Hello Thomas,
Thank you for the inputs.
Please refer below threads. I guess you will be using the PRU to implement the Ethercat. I assume the CPSW is available.
https://www.ti.com/product/AMIC110#hardware-development
https://www.ti.com/tool/TIDA-00299 …
Part Number: DP83822IF Other Parts Discussed in Thread: TIDA-00299 Hi all Would you mind if we ask DP83822IF? On TIDA-00299, Reset pin pull down resistance is 2.4kohm. Is it possible to use 10kohm for pull down? Does it use for low level in case of indefinite…
Hello AbdelRahman Ahmed,
Thank you for the query and sorry to not the non availability of the solutions and he devices you are looking for.
TI does not provide switch solution.
Please refer below to implement a dual Ethernet solution
https://www.ti.com…
Hello Wendy,
Thank you for the reply.
Not sure if you previously looked at the below designs
https://www.ti.com/tool/TIDA-00299
https://www.ti.com/tool/TIDM-DELFINO-ETHERCAT
DP83822 offers optimal solution for copper or fiber interface.
Regards,
Sree…
Hi Steve,
The reference designs we have available are under the "Design and Development" tab of the product folder. I believe the following may be useful:
http://www.ti.com/tool/TIDA-00299
http://www.ti.com/tool/TIDA-00928
Thank you,
Nikhil …
Part Number: AM3352 Other Parts Discussed in Thread: TIDA-00299
Hi,
a customer is connecting 2x DP83822 PHYs on the 2x PRU MII interfaces and wants to configure two things on bootup
[] Put the AM3352 into 25MHz crystal mode via SYSBOOT[15:14] = 10b…
Hi Wassim,
You are correct, the pin out is different between TLK111 and DP83822I. It's a incorrect tagging on our product page and I will get that fixed. Thanks for pointing it out.
DP83822I supports the similar functionality as TLK111 and is qualified…
Hi Sandesh,
We do not have application notes like this.
We do provide reference designs that show the DP83822 connected to microprocessors with integrated MAC layers.
For example, see the TIDA-00299 design here: www.ti.com/.../TIDA-00299
Best Regards…
Part Number: AMIC110 Other Parts Discussed in Thread: TMDXICE110 , TIDA-00299 ,
Hi,
My customer would like to evaluate the AMIC110. They found the TIDA-00299 reference design which looks identical to the TMDXICE110 EVM. Can you confirm these are identical…