Part Number: TIDA-00365 Other Parts Discussed in Thread: SM72295 , Hi,
I have used the reference design TIDA-00365 to design motor controller for brushed DC motors, I ran the motors with 16KHz PWM signal via SM72295 and through the H-Bridge at different…
Part Number: TIDA-00365 Other Parts Discussed in Thread: SM72295 , Dear expert:
Can you kindly find the design guideline please? Can you teach me how to select D4 of Figure6?
Is D4 also used to protect against motor Induced electromotive force?
Thanks! …
Dear Santosh,
Your initial question was if TIDA-00365 can be used for to convert 12V PWM to 75V. Your last answer was that you need a minimum 55V, and TIDA-00365 supports 75V, hence meet that. As I wrote in my first answer, the limitation is that the…
Hello Lorenzo,
It is possible assuming the driver is operating within the recommended operating conditions.
TIDA-00365 uses a different driver but it is applicable to the UCC27289.
Regards,
-Mamadou
Hello Mamadou,
Thanks for reply!
If I design the brushed DC drives based on the demo board TIDA-00365 .This MOSFET CSD19534Q5A is on the demo board .
It means that : Psw = Qg * VDD * Fsw = 22nc *12V * 500KHz = 0.132W ?
Tj = (P * RθJA) + Ta = 0.132W * 60…
Hi,
I have this kit TMDSDOCK28035 , can we use it to program the card enstead the Launchpad, and do you have this card available TIDA-00365( http://www.ti.com/tool/TIDA-00365#0 )? if is it available I'll buy it.
thanks.
Hello Maynard,
Thank you for checking with us. I assume you refer to a single-phase brushed PMDC motor and not a single-phase brushless DC motor?
We don’t have an integrated solution for >60V brushed DC motors and I’ll list below what we have.…
Hello Manoj,
I've sent an email them to prevent their burnt issue with below articles. But not received the response from customer side yet.
- <checklists> Uniflash do not have much differences than CCS debug mode.
but, please check below…