Part Number: TIDA-00367 Tool/software: WEBENCH® Design Tools we use your IC(UCC28630) to design one playback, and study your reference design(TIDA-00367),and find the below formula:
the power dissipated in the snubber circuit(RCD): P_SN=0.5 x L_leak x…
Part Number: TIDA-00367 Hi,
Looking at TIDA-00367, there appears to be quite some confusion prevailing around. The pdf schematic shows:
That said, the Altium schematic shows:
Even more stranger, the BOM
states the following, which does not…
Hi Ram,
Accidentally came up on this document from Ray Ridley:
Looking from the description given on Page #7 High noise and Low noise configuration;
In TIDA-00367,
W1 starts at Pin 1, ends at Pin 2; Pin 1 is the switching node
W2 starts at Pin 8, ends…
Part Number: TIDA-00367 In below picture where i mentioned red color question mark (?) , in my hardware voltage continuously vary, not stable due to this UCC-28630 not "ON"
Part Number: TIDA-00367 Tool/software: WEBENCH® Design Tools Hello,
I'd like to know how may I change the output configuration of 24V 6.25A to 12V 12,5A of TIDA-00367 .
Probably I have to re-design the transformer.
May you help me with this.
Thanks …
Part Number: TIDA-00367 Sir ,
I want to know about the power factor of TIDA-00367 and availability of this part no.
or suggest any other design for 24V-6A AC-DC SMPS.
Thank You .
Part Number: TIDA-00367 HI,
Any idea what happened to this post ?
There wasn't any response to the post. The thread appears to be locked.
Any idea ?
Thanks,
Manu
Part Number: TIDA-00367 Hi,
Following up on this thread
Regarding W1, the manufacturer is short on 26AWG wire. As a result, the following feedback he has:
We don't have Tex-E wire 26 AWG (0.40mm), but we have 0.25mm & 0.60mm Tex-E in stock. Either…