Part Number: TIDA-00476 Ramkumar S
in source file this part in case MPPT_STATE:
// value 10 corresponds to approximately .12A //This block has to change RAM
if(!Wait_State) {
if((Battery_Charging_Current < 24) ) {
Battery_Low_Current_Counter…
Part Number: TIDA-00476 Other Parts Discussed in Thread: UCC28880 I want to use the reference design TIDA-00476 . For my project I need to change some things in the firmware but the files I need to modify are located into the TIDA-00476 _LIBR.lib file.…
Part Number: TIDA-00476 I want to use this design for 22/44V panels but when I connect a 44V panel Q2 is blown-up. I did somes test with less powerfull sunlight and it seems to work, but now when rhe sun is more powerfull Q2 blown-up. With one board also…
Part Number: TIDA-00476 In the discription of TIDA-00476 I read:
" The same power stage can be operated as a synchronous boost to drive a DC load with configurable constant current and constant voltage limits (CC/CV)"
The only things I can change…
Part Number: TIDA-00476 Other Parts Discussed in Thread: MSP430F5132 I want to use the reference design TIDA-00476. This is my first attemp to work with the MSP430F5132IDAR controller. For my use I need to change something in the software but I can't find…
Hi Ram,
I'm now ready with the changes, I have learned a lot from this design, and created a streamlined to my wishes perfect working design.
Thanks for you help,
Rob
Part Number: TIDA-00476 Other Parts Discussed in Thread: UCC28880 , CSD88539ND , Testing with a power supply goes very well, no problems at all. But connected to a solar panel in the real world gives problems.
After charging is finish it can happen that the…
Other Parts Discussed in Thread: TIDA-00476 , PMP21529 , LM5170-Q1 , PMP22650 , UCD3138 Hello Ti, we have a project where we want to simulate how EV’s can use their battery to stabilize the power grid. It should be just a simulation of a real system (only…
Can I get to know who is the owner of TIDA 00476?
One of my customer wants to develop power optimizer for Solar energy and our competitor already promoted solution with $7.xx.
To estimate performance, I need TIDA 00476 board.
And need to discuss with…