Other Parts Discussed in Thread: TIDA-00476 Hi,
I was going with the reference design of TIDA-00476 and on page 6 of the reference design i came across line which details the protection features that is incorporated in this design. it says "The system provides…
Hi Salil,
Thanks for the reference designs. TIDA-00476 may prove to be useful in my application. However, what I am interested in is a device that can simultaneously allow part of a solar arrays power to be delivered to a DC load and the rest of the power…
Part Number: TIDA-00121 Other Parts Discussed in Thread: TIDA-00476 Hi,
The Design TIDA-00121.As mentioned TI,It is possible to increase the LED Drive current up to 1.1A.
We need the LED drive current up to 2A.
Please suggest the hardware changes required…
Part Number: TIDA-00120 Other Parts Discussed in Thread: TIDA-00121 , TIDA-00476 Hi,
My customer is working on a 500W solar charge controller and would like to know if they could parallel 4x TIDA-00120. I would think the MPPT circuitry would ensure each…
Part Number: TIDA-00121 Other Parts Discussed in Thread: TIDA-00476 Hii Expert
The Design TIDA-00121 Solar Street Light Integrated MPPT design output current to LED Driver is 700 mA. U have already mentioned that it can be improved upto 1.1A by some hardware…
Howard,
TPS40345 is not a bidirectional converter. It is only a buck controller. Please see this reference design as an example:
www.ti.com/.../TIDA-00476
Pão,
We actually have several designs that might serve you well as a starting point.
Please take a look at the following design examples:
http://www.ti.com/tool/TIDM-BUCKBOOST-BIDIR
http://www.ti.com/tool/TIDA-00476
http://www.ti.com/tool/TIDA…
Part Number: TIDA-010042 Other Parts Discussed in Thread: TIDA-00121 , , TIDA-00476 Hi All,
I am evaluating the TIDA010042 module for one of my upcoming project.
I am facing an issue with the charging functionality.
Please clarify it.
Condition: a. 12V battery…