Part Number: TIDA-00771 Other Parts Discussed in Thread: TIDA-00772 Hallo,
Could you please send me Altium Designer project file for the reference design TIDA-00771 ?
There is no altium project files added in the reference design.
my Email: xiaofeng…
Other Parts Discussed in Thread: TIDA-00771 1. What is R11 in the below pic used for? How to determine the value of R11?
2. What's R6 and R7 used for? How to determine the value.
Thanks.
Other Parts Discussed in Thread: MSP430G2553 Hi, I'm reading the firmware of TIDA00771.
I found that the SPI is implemented with four IO ports, not the SPI module in MSP430G2553, why?
Moreover, the readregister function is as below:
uint16_t ReadRegister…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: TIDA-00643 , TIDA-00771 , BOOSTXL-DRV8305EVM Hi all
My customer has this question for the DRV8305-Q1:
What is the output drive capability of the current sense amplifiers ?
Please find the customer…
Hi Alexey,
I do not see any specifications in the DRV8305 datasheet which cannot be met by the MSP430FR5994. TIDA-00645 and TIDA-00771 even use a MSP430G2553 and DRV8305. Please post logic analyzer or oscilloscope screenshots of the SPI communication…
Hi, Nick,
In fact, i did some mistake, sorry for it. I saw this in TIDA-00771, ( www.ti.com/.../TIDA-00771 . It is nornal to expect inverting, I thought that there is something else in DRV8305. It's alright now.
The BOOSTXL-DRV8301 was designed to work with an LaunchPad XL (of which the MSP-EXP430G2 is not) and there is no MOTORWARE support for MSP430 devices that I know of, except perhaps some preliminary work with the MSP430FR5739. There are however several…