Hi James,
We do not have an IC similar to the GC12, but we do have a Reference Design that performs a similar function: http://www.ti.com/tool/TIDA-00796 :
Automotive Resolver-to-Digital Converter Reference Design for Safety Application
.
Please review…
Part Number: PGA4311EVM Other Parts Discussed in Thread: PGA411-Q1 , SYSCONFIG , LAUNCHXL-F28379D
Hellow
I am having the same issue that Vish Raman had faced in his original thread where any command request is responding with a message like 0x46. Can…
Part Number: TMDSCNCD28035ISO Other Parts Discussed in Thread: TMS320F28035 , , PGA411-Q1 , CONTROLSUITE Tool/software: TI C/C++ Compiler Hello,
after building a project i get the message
undefined first referenced symbol in file --------- ----------…
Part Number: PGA4311EVM Other Parts Discussed in Thread: PGA411-Q1 , SYSCONFIG , LAUNCHXL-F28379D
I every one
I am interfacing pga411 with f28379d launchpad
when I started debugging the code, I am facing an issue with the void pga411_DefaultCfg(void) function…
Zubair,
Do you have access to an oscilloscope? You should check that the analog signals look OK.
- OE1 and OE2
- IE1 and IE2
- IZ1, IZ2, IZ3, and IZ4
- OCOS and OSIN
The "Troubleshooting Guide for PGA411-Q1" includes images of what these signals typically…
We have a few resources ready for this.
- Example firmware for the C2000 is available in this TI design: www.ti.com/.../TIDA-00796
- Documentation for the firmware is in this app note: www.ti.com/.../slaa708
- Step-by-step documentation for connecting…
thank you for replay,
I use the demo of 28069 , which is called "TIDA-00796-LIGHT",
the exciter and sin ,cos are OK, but there are no singles from OUTA/OUTB.
Rich,
We do not have immediate plans to create an API for the PGA411-Q1 EVM. The current EVM/GUI has limitations with how fast it can stream angle data, so it might not be that useful for data analysis purposes anyways.
It might be useful to look at…
Vincent,
The PGA411 GUI does support a streaming option; however, the sample rate may not be fast enough for you. If you need a faster and more consistent sample rate, then you could use the sample code available in the automotive TI design as a starting…
Hi All
Is this are available on ti store?
www.ti.com/.../TIDA-00796
Automotive Resolver-to-Digital Converter Reference Design for Safety Application
(ACTIVE) TIDA-00796
Is it the only one tools ported on F28069M LanuchPad?
Regards,
Hank