Part Number: TIDA-00893 Other Parts Discussed in Thread: ISOW7841 , TCAN1042-Q1 , SN65HVD256 Hello,
Our customer trying isolated can circuit based on TIDA-00893.
We can see that ISOW7841 can supply 130mA max to load in this.
However, TCAN1042 requires 180mA…
Dear Santosh,
thanks for your quick answer,
the configuration of the jtag is correct.
Yesterday we found a schematic issue: we connected a ISOW7841 (tida 00893) supplied at 5V to one microcontroller's GPIO (the voltage on the pin was 4.6V),
we, in…
Part Number: ISOW7841 Other Parts Discussed in Thread: TIDA-00893 Hi Sir,
Our customer used the ISOW7841, But EMI report Fail.
Could you please support for Review Layout?
or based on EMI report Could you please provide the suggest for me?
Hugo
108-01…
Other Parts Discussed in Thread: SN65HVD232 , ISO7721 , ISO1050 , TIDA-00893 Hi Sirs,
We are looking for CAN Isolator .
The CAN transceiver is SN65HVD232.
Does TI have suitable CAN Isolator can share for us (ISO7721) ?
We couldn't use ISO1050 because our VrefA…